It depends on the gateway specifications which is usually defined by the number of packets it can support.
For instance, if there is a 8-channel Gateway supporting 1.5M packets/day, and if the application sends 1 packet per hour, then more than 62,000 nodes can be handled by that Gateway.
Theoretically, mesh topology is possible. However, LoRa is defined for star-topology only.
Return to LoRa Module Page
Back to LoRa FAQ List